AXIS#.MOTOR.TEMPFAULT
Description
This parameter is used to configure the motor temperature fault level as a resistance threshold of the motor thermal sensor
A sensor is a type of transducer that converts one type of energy into another for various purposes including measurement or information transfer.
A zero value prevents temperature faults from being reported.
-
-
This parameter is automatically configured for Kollmorgen motors when AXIS#.MOTOR.AUTOSET = 1 and motor memory version is 0.3 or greater.
Context
For more information see Motor.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read/Write |
|
Units |
Ω |
|
Range |
0 to 2,000,000,000 Ω |
|
Default Value |
2000 |
|
Data Type |
Integer |
|
See Also |
|
|
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Fieldbus Information
| Fieldbus |
Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO Mappable |
|---|---|---|---|---|---|---|---|---|
| EtherCAT |
AXIS1.MOTOR.TEMPFAULT | 0x500B | 0x1D | UDINT | - | - | RW | False |
| AXIS2.MOTOR.TEMPFAULT | 0x510B | 0x1D | UDINT | - | - | RW | False |